AXIS#.IL.COMPTABLE.INPUT

Description

The input position (after modulo) in the cogging compensation block. This value is only valid when the compensation table is active (AXIS#.IL.COMPTABLE.ENABLE is 1).

Versions

Action Version Notes
Implemented 02-08-02-000

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float
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
AXIS1.IL.COMPTABLE.INPUT

500ah

28h

Signed32

Position

-

Read only

No

AXIS2.IL.COMPTABLE.INPUT

510ah

28h

Signed32

Position

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.COMPTABLE.INPUT

5845

16D5

Signed32

Read Only

Position

AXIS2.IL.COMPTABLE.INPUT

71381

116D

Signed32

Read Only

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COMPTABLE.INPUT

5845

Signed32

Read Only

Position